適切なPLC/DCSシグナル・チェーン構成を選択するには、精度、帯域幅、入力レンジなど、さまざまなシステム条件を考慮する必要があります。アナログ・デバイセズの優れたアプリケーション・エンジニアが、150種類を超える特別に準備したソリューションによって設計プロセスを支援いたします。これらのソリューションは、業界最高レベルの技術を搭載し、ディスクリート部品の実装から完全に統合されたソリューションまで、電源の選択も含め、ありとあらゆる豊富な設計オプションを提供します。アナログ・デバイセズのエンベデッド・プロセッシング&DSP製品、ソフトウェア、リファレンス・デザイン、その他の詳細については、「Processors for Industrial & Process Control」のホームページをご覧ください。完全なPLCデモ・システムも見ることができます。
このサイトをご覧になるには、IE7+, Firefox 3.0+ および Chrome 2.0+ をおすすめします。 IE6 でもご覧いただけますが、画面が完全に表示されるまでに時間がかかる場合があります。
SELECT A SOLUTION
Isolated 12 bit voltage output, using AD5621, ADTL082, ADR02 to program the following ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24v Supply
Isolated 12 bit voltage output, using AD5620 and AD5750-1, ADR02 to program the following ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24v Supply
Isolated 12 bit voltage output, using AD5412 to program the following ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24v Supply
Isolated 16 bit voltage output, using AD5660 and AD7793 to program the following ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24v Supply
Isolated 16 bit voltage output, using AD5422 to program the following ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24v Supply
Isolated 12 bit, 4 channel voltage output, using AD5624, ADR02, ADTL082 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24V input supply.
Isolated 12 bit, 4 channel voltage output, using AD5624 quad 12 bit DAC, and 4 X AD5750-1 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24V input supply.
Isolated 12 bit, 4 channel voltage output, using AD5724 quad 12 bit DAC, to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24V input supply.
Isolated 16 bit, 4 channel voltage output, using AD5664, ADR02, OP2177 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24V input supply.
Isolated 16 bit, 4 channel voltage output, using AD5664 quad 16 bit DAC, and 4 X AD5750-1 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24V input supply.
12 bit, 4 channel voltage output, using AD5624, ADR02, ADTL082 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v).
12 bit, 4 channel voltage output, using AD5624 quad 12 bit DAC, and 4 X AD5750-1 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v).
12 bit, 4 channel voltage output, using AD5724 quad 12 bit DAC, to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v).
16 bit, 4 channel voltage output, using AD5664, ADR02, OP2177 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v).
16 bit, 4 channel voltage output, using AD5664 quad 16 bit DAC, and 4 X AD5750-1 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v).
16 bit, 4 channel voltage output, using AD5754 quad 16 bit DAC, to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v).
Isolated 12 bit, 8 channel voltage output, using AD5628 octal 12 bit DAC, and external amplifiers OP2177 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24V input supply.
Isolated 12 bit, 8 channel voltage output, using AD5628 octal 12 bit DAC, and external amplifiers OP2177 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24V input supply.
Isolated 16 bit, 8 channel voltage output, using AD5668 octal 16 bit DAC, and external amplifiers OP2177 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24V input supply.
Isolated 16 bit, 8 channel voltage output, using AD5668 quad 16 bit DAC, and 4 X AD5750-1 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24V input supply.
12 bit, 8 channel voltage output, using AD5628 octal 12 bit DAC, and external amplifiers ADTL082 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v).
12 bit, 8 channel voltage output, using AD5628 octal 12 bit DAC, and 4 X AD5750-1 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v).
16 bit, 8 channel voltage output, using AD5668 octal 16 bit DAC, and external amplifiers OP2177 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v)
16 bit, 8 channel voltage output, using AD5668 quad 16 bit DAC, and 8 X AD5750-1 to program the following voltage ranges (0-5v, 0-10v, +/-5v, +/-10v).
Isolated 12 bit current output, using AD5621, ADR02, AD822 to program the following ranges 4-20ma. Includes Power Management solution from 24v Supply
Isolated 12 bit current output, using AD5620 and AD5750-1 to program the following ranges (4-20ma, 0-20ma, 0-24ma). Includes Power Management solution from 24v Supply
Isolated 12 bit current output, using AD5412 to program the following ranges (4-20ma, 0-20ma, 0-24ma). Includes Power Management solution from 24v Supply
Isolated 16 bit current output, using AD5662, ADR02, AD822 to program the following ranges 4-20ma. Includes Power Management solution from 24v Supply
Isolated 16 bit current output, using AD5660 and AD5750 to program the following ranges (4-20ma, 0-20ma, 0-24ma). Includes Power Management solution from 24v Supply
Isolated 16 bit current output, using AD5420 to program the following ranges (4-20ma, 0-20ma, 0-24ma). Includes Power Management solution from 24v Supply
Isolated 12 bit, 4 channel current output, using AD5624 quad 12 bit DAC, and external amplifiers OP2177 to program the following current ranges (4-20ma, 0-20ma, 0-24ma). Includes Power Management solution from 24V input supply.
Isolated 12 bit, 4 channel current output, using AD5624 quad 12 bit DAC, and 4 X AD5750-1 to program the following current ranges (4-20ma, 0-20ma, 0-24ma, +/-20ma). Includes Power Management solution from 24V input supply.
Isolated 16 bit, 4 channel current output, using AD5664 quad 16 bit DAC, and 4 X AD5750-1 to program the following current ranges (4-20ma, 0-20ma, 0-24ma, +/-20ma). Includes Power Management solution from 24V input supply.
12 bit, 4 channel current output, using AD5624 quad 12 bit DAC, and external amplifiers AD822 to program the following current ranges (4-20ma, 0-20ma, 0-24ma, +/-20ma).
12 bit, 4 channel current output, using AD5624 quad 12 bit DAC, and 4 X AD5750-1 to program the following current ranges (4-20ma, 0-20ma, 0-24ma).
16 bit, 4 channel current output, using AD5664 quad 16 bit DAC, and external amplifiers AD822 to program the following current ranges (4-20ma, 0-20ma, 0-24ma).
16 bit, 4 channel current output, using AD5664 quad 16 bit DAC, and 4 X AD5750-1 to program the following current ranges (4-20ma, 0-20ma, 0-24ma, +/-20ma).
Isolated 12 bit, 8 channel current output, using AD5628 octal 12 bit DAC, and external amplifiers AD822 to program the following current ranges (4-20ma, 0-20ma, 0-24ma). Includes Power Management solution from 24V input supply.
Isolated 12 bit, 8 channel current output, using AD5628 quad 12 bit DAC, and 4 X AD5750-1 to program the following current ranges (4-20ma, 0-20ma, 0-24ma, +/-20ma). Includes Power Management solution from 24V input supply.
Isolated 16 bit, 8 channel current output, using AD5668 octal 16 bit DAC, and external amplifiers AD822 to program the following current ranges (4-20ma, 0-20ma, 0-24ma). Includes Power Management solution from 24V input supply.
Isolated 16 bit, 8 channel current output, using AD5668 quad 16 bit DAC, and 4 X AD5750-1 to program the following current ranges (4-20ma, 0-20ma, 0-24ma, +/-20ma). Includes Power Management solution from 24V input supply.
12 bit, 8 channel current output, using AD5628 octal 12 bit DAC, and external amplifiers AD822 to program the following current ranges (4-20ma, 0-20ma, 0-24ma,).
12 bit, 8 channel current output, using AD5628 quad 12 bit DAC, and 4 X AD5750-1 to program the following current ranges (4-20ma, 0-20ma, 0-24ma, +/-20ma).
16 bit, 8 channel current output, using AD5668 ocatl 16 bit DAC, and external amplifiers AD822 to program the following current ranges (4-20ma, 0-20ma, 0-24ma).
16 bit, 8 channel current output, using AD5668 quad 16 bit DAC, and 4 X AD5750-1 to program the following current ranges (4-20ma, 0-20ma, 0-24ma, +/-20ma).
Isolated 12 bit V/I output, using AD5621, OP2177, AD822 to program the following ranges (4-20ma, 0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24v Supply
Isolated 12 bit V/I output, using AD5620 and AD5750-1, ADR02 to program the following ranges (4-20ma, 0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24v Supply
Isolated 12 bit V/I output, using AD5412 to program the following ranges (4-20ma, 0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24v Supply
Isolated 16 bit V/I output, using AD5662, OP2177, AD822 to program the following ranges (4-20ma, 0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24v Supply
Isolated 16 bit V/I output, using AD5422 to program the following ranges (4-20ma, 0-5v, 0-10v, +/-5v, +/-10v). Includes Power Management solution from 24v Supply
Isolated 12 bit, 4 channel V/I output, using AD5624 quad 12 bit DAC, and external amplifiers OP2177, AD822 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma, +/-20ma). Includes Power Management solution from 24V input supply.
Isolated 12 bit, 4 channel V/I output, using AD5624 quad 12 bit DAC, and 4 X AD5750-1 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma, +/-20ma). Includes Power Management solution from 24V input supply.
Isolated 16 bit, 4 channel V/I output, using AD5664 quad 16 bit DAC, and external amplifiers OP2177, AD822 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma, +/-20ma). Includes Power Management solution from 24V input supply.
Isolated 16 bit, 4 channel V/I output, using AD5664 quad 16 bit DAC, and 4 X AD5750-1 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma, +/-20ma). Includes Power Management solution from 24V input supply.
4 channel V/I output, using AD5624 quad 12 bit DAC, and external amplifiers OP2177, AD822 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma, +/-20ma).
12 bit, 4 channel V/I output, using AD5624 quad 12 bit DAC, and 4 X AD5750-1 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma, +/-20ma)
4 channel V/I output, using AD5626 quad 16 bit DAC, and external amplifiers OP2177, AD822 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma, +/-20ma).
4 channel V/I output, using AD5664 quad 16 bit DAC, and 4 X AD5750-1 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma, +/-20ma).
Isolated 12 bit, 8 channel V/I output, using AD5628 octal 12 bit DAC, and external amplifiers OP2177, AD822 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma). Includes Power Management solution from 24V input supply.
Isolated 12 bit, 8 channel V/I output, using AD5628 quad 12 bit DAC, and 4 X AD5750-1 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma, +/-20ma). Includes Power Management solution from 24V input supply.
Isolated 16 bit, 8 channel V/I output, using AD5668 octal 16 bit DAC, and external amplifiers OP2177, AD822 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma). Includes Power Management solution from 24V input supply.
Isolated 16 bit, 8 channel V/I output, using AD5668 quad 16 bit DAC, and 4 X AD5750-1 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma, +/-20ma). Includes Power Management solution from 24V input supply.
12 bit 8 channel V/I output, using AD5628 octal 12 bit DAC, and external amplifiers OP2177, AD822 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma).
12 bit, 8 channel V/I output, using AD5628 octal 12 bit DAC, and 8 X AD5750-1 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma, +/-20ma)
16 bit 8 channel V/I output, using AD5668 octal 16 bit DAC, and external amplifiers OP2177, AD822 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma).
16 bit 8 channel V/I output, using AD5668 octal 16 bit DAC, and 8 X AD5750-1 to program the following voltage and current ranges (0-5v, 0-10v, +/-5v, +/-10v, 4-20ma, 0-20ma, 0-24ma, +/-20ma).
ADUM540X isolated 5V to 5V supply, includes Digital Isolation.
Isolated 5V to +/-15v Supply using ADP1621.
Isolated 5V to +/-24v Supply using ADP1621.